Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

can't be complied successfully

Hi , i try to run the CLK example from STM8L15x_StdPeriph_Examples, but i can't compile the project successfully , below is my procedure, can you help it?create a new workspace using STVD tooladd the source and head files from the STM8L15x library f...

ALiu.5 by Associate II
  • 1650 Views
  • 3 replies
  • 0 kudos

Alternative Debuggers for STM8

Hi :)So I've been using the lovely software provided by ST, called ST Visual Develop, which is, not only one of the worst IDE I have ever encountered (I quickly switched to writing the actual code in another editor), but also is full of so many bugs....

SLasn.1 by Senior
  • 908 Views
  • 1 replies
  • 0 kudos

Update for STM8 Bootloader Manual (UM0560)...?

the STM8 bootloader manual (UM0560 rev10) appendix B describes fewer families/bootloader versions than the erase/write RAM routines bundled with the FLASHER-STM8 v2.8.0. Specifically the newer BL versions v2.4 and v1.4 are missing, as well as the 256...

GIcki by Associate II
  • 803 Views
  • 0 replies
  • 0 kudos

Resolved! How to find a copy of Application Note AN433

I'm helping a friend fix his battery charger. The Micro processor in it is a ST6200. Its spec has a list of Application Notes including the AN433. But a search of the ST web site failed to find it - which seems odd. Any assistance will be appreciated...

LCox.2 by Associate
  • 1395 Views
  • 2 replies
  • 0 kudos

stm8s CCORDY on CCOR register never set

hi friends i asked my question just a few days ago but nobody answerd i dont know what should i do when i configure micro controller for cco output it generates out put of course its a little unaccurate when i check that is cco stable by checking CCO...

akhan.1 by Associate II
  • 525 Views
  • 0 replies
  • 0 kudos