Why did Viper113XS removed from eDesignSuite?Is there a problem about IC? I need to know that because I made a design and ordered the IC, if IC has some problems I need to change it.
I need to calculate the analog compensator values so I need to know pwm ramp voltage of sg3525 but I cant find on datasheet, can somebody help me about it?
I have a 85-265AC input and desired to have 5 volt output buck converter.How can I make the viper265kd to perform 5V output?When I check AN5380 the VDD is supplied by output voltage which is 15V and it's enough to supply VDD min requirements.I need 5...