User Activity

Hi,for a product I want to activate read-out-protection (ROP) via option byte, to prevent misuse via the SWIM interface. However, is it possible to disable it again from the application (given a "secret" condition)? Page 50 in RM0016 indicates that A...
the STM8 bootloader manual (UM0560 rev10) appendix B describes fewer families/bootloader versions than the erase/write RAM routines bundled with the FLASHER-STM8 v2.8.0. Specifically the newer BL versions v2.4 and v1.4 are missing, as well as the 256...
Hi,I am the author of an OS tool flash tool named "stm8gal" for programming the STM8 via the ROM bootloader. Currently I check family type and memory size by probing different addresses. This is extremely ugly and may fail in devices I couldn't test ...
I am looking for an CAN bus example for the STM8A discovery board. App Note 4178 (LIN example) refers another App Note (4179) for a respective CAN example. However, I can't find it on st.com - nor can I find a suitable example via Google. Can someone...
hello all,I am currently trying to add STM8 peripherals to the Eclipse embsysregview plugin. For this I would need device descriptions in XML or SVD. For STM32 ARM devices these are published as SVD files (see e.g. https://www.st.com/content/st_com/e...
Kudos from