Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
Dear Sir,I need a datasheet for part number: 1826-6579I would be glad to help me.Kind regardsSaeed
Hello,I have a x-nucleo-idw01m1 and i'm trying to update it's firmware... Reading online i figured out that the latest version is 3.6 but i cannot happen to find the binary image anywhere, all of the links provided are broken.Does somebody still have...
I'm currently using the STM8L151F3 and implementing the SUMP open logic analyzer. In one part of my code involving with GPIO reading and send data to SPI1_DR. and to make a lots of the capture samples, I use the F-RAM as a external RAM for sampling m...
Im using the COSMIC Toolchain with the standard library.Here is the setting:##########################################################void clock_init(void){ CLK_DeInit(); CLK_HSECmd(DISABLE); CLK_LSICmd(DISABLE); CLK_HSICmd(ENABLE); whi...
Hello, I have a strange problem with STVD. The changes to the project are not saved. After closing and openning the project, non of the changes are saved. I appreciate any help. Best regards
When debugging erro occurres "Failed to launc child process: <gdb.exe> > error = 2- the system cannot find the file specified.Using:W10ST Visual DevelopSTM8S003F3P6Is there any solution to this problem?
How can I download the full datasheet of STHV800.+
We use STM8 micro for one of our projects and the ST Visual Developer for the development environment. We are in need of debugging some of our units for warranty return analysis and ST visual developer is giving weird errors stating not able to detec...