cancel
Showing results for 
Search instead for 
Did you mean: 

HVLED001 eDesignSuite vs Datasheet

ppereira
Associate II
Posted on November 14, 2016 at 19:03

Hi There,

After using the eDesignSuite to design a 25V (CV / HPF / PSR) using the HVLED001, we found some discrepancies between the eDesignSuite proposed circuit and the HVLED001 typical HPF / PSR / CV circuit on page 16 of the datasheet. Especifically on:

- components connected to pin ZCD

- the place where RtOff connects (between Cs, RS on eDesignSuite and pin FB on datasheet)

- zener on clamper (datasheet) -> no zener on eDesignSuite

Which one is right?

We really need help on this since we must do the PCB prototypes ASAP.

Best Regards,

#hvled001 #edesignsuite #datasheet
This discussion is locked. Please start a new topic to ask your question.
7 REPLIES 7
Patrizia BELLITTO
ST Employee
Posted on November 15, 2016 at 12:51

Hello Pedro,

could you export your design from eDesignSuite and send it to us? The application engineer responsible for this device could have a look and verify if everything is correct.

In the meanwhile, you could read this new application note, with a lot of explanations about the HVLED001A applications

http://www.st.com/content/ccc/resource/technical/document/application_note/group0/ba/21/1d/6d/45/f6/43/36/DM00335810/files/DM00335810.pdf/jcr:content/translations/en.DM00335810.pdf

Best regards,

Patrizia

ppereira
Associate II
Posted on November 15, 2016 at 18:53

Hi There Patrizia,

Please find attached the files (from eDesignSuite) of the power supply we are currently designing so that you can check the discrepancies. Thanks in advance.

________________

Attachments :

ps_257.prj : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzEd&d=%2Fa%2F0X0000000bIg%2FlBUorFv_a0LdhmqSfdEPJYXamwKx4rIOEn6o0i3MgHw&asPdf=false
Patrizia BELLITTO
ST Employee
Posted on November 16, 2016 at 11:44

Hi Pedro,

the design and the schematic from your project are correct. We found a small error in the schematic, the GND is missing on the secondary, but we'll fix it in the next release.

We suggest you to review the values of input capacitor and filter during the debug phase of the prototype, but for the rest you can follow the BOM and the schematic you created with eDesignSuite.

Best regards,

Patrizia

ppereira
Associate II
Posted on November 16, 2016 at 13:46

Thanks for the support Patrizia. The value of the coupling capacitor between aux ground and secondary ground is also missing.

ppereira
Associate II
Posted on November 18, 2016 at 11:36

Hi There Patrizia,

While selecting components for the prototype a doubt arose. The Cclp Polypropylene (PP) 150pF capacitor rated 400V on BOM should be 400VDC ou 400VAC? Because when selecting capacitors a 400VDC is usually only 250VAC. Does 400V mean 400VAC or 400VDC?

Best Regards,

Pedro Pereira 

Patrizia BELLITTO
ST Employee
Posted on November 21, 2016 at 09:19

Hello Pedro,

the capacitor voltage ratings are expressed in VDC.

Best regards,

Patrizia

ppereira
Associate II
Posted on November 21, 2016 at 11:23

OK.

Thank you Patrizia.