Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
I need a formal MTBF/FIT/Reliability report for the subject PN for my product life prediction. Thanks.I need to see the FIT's at different confident levels, temperatures, ..etc. Is there a site link I can obtain the data similar your competitors offe...
Here's the issue. I have built a LIN bus with a slave node and a master node using tow STM8AF/AL-Discovery boards. After flashing the boards with the demo of the STM8 LIN driver 5.1 as slave node and master node I can control either the LED or the b...
Hi,I generate 2 mhz from the PORT / PIN C4 (CCO).The problem is that instead of a square signal, I get a triangle signal.What could be the reason????On PORT / PIN A3 i can generate a square signal, but not on C4I Use the STM8-SO8-DISCO Board in which...
I am using an IAR compilation environment, the microcontroller is STM8S105C4T6, but in the clock initialization, CLK__CKDIVR=0x00; the CLK__CKDIVR in this sentence keeps prompting that this function cannot be found.And it is the same when initializin...
We have this part LD1117S18CTR and the top side marking is LD18 but we cannot find this listed anywhere on the data sheet to confirm that we have the correct parts on the board that we just build. We are making our AOI program and need this info t...
I have just come back to STVD after a long while (and various changes of machine) and have reinstalled STVD and COSMIC. I can now compile my existing code but when trying to link it during the build process I get a page of errors like;#error clnk Rel...