Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VN340SP-E Conformity to IEC 61131-2

Hello,It is stated that the VN340 has conformity to IEC 61131-2.At what manner does it have the conformity? At EMC? At safety? At UL? It is not clear at all from the datasheet and from the site.Best regards,Asaf Abraham

AAbra.4 by Associate
  • 909 Views
  • 0 replies
  • 0 kudos

Resolved! Which software can I use the OUT extension?

https://www.st.com/en/embedded-software/stsw-viennarect.html?ecmp=tt9470_gl_link_feb2019&rt=db&id=DB4073The content of the file that can be obtained with GET Software in is the extension OUTI want to write "stsw-viennarect.out" to STNRG388A. Which so...

HKOBA.1 by Associate II
  • 5209 Views
  • 7 replies
  • 0 kudos

CENTERALIGNED pwm not working

iam using stm8s003f3 microcontroller i configured centeraligned pwm but not workingattached wave form also please suggest.void TIM1_setup(void){   TIM1_DeInit();            TIM1_TimeBaseInit(0, TIM1_COUNTERMODE_CENTERALIGNED3 , 1000, 0);      TIM1_BD...

0693W00000D17WcQAJ.jpg
gm.1 by Associate
  • 1001 Views
  • 0 replies
  • 0 kudos

products supply

I usually use STM8L151C8T6 micro-controller.But it's difficult to get it.What does ST Micro think the major/main products on STM8 CPUs families?Should I change the micro-controller from STM8L151C8T6?So, what kind of families should I use?Please tell ...

YIshi.1 by Associate II
  • 1524 Views
  • 2 replies
  • 0 kudos

Resolved! How to select pages on M24512

Hello,I am a automotive firmware developer.I'm developing using the M24512-DRMN3TP/K product.I have a question.I have used the FM24CL16B (AT24/FM24) model before.FM24CL16B model had 1010+page select in SLAVE ADDRESS.I was able to fully understand the...

Skim.3 by Associate
  • 1363 Views
  • 1 replies
  • 0 kudos