Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Stop iwdg in halt mode on STM8L051F3

HeyI have tried to use the option byte to stop the iwdg when i enter halt.I can see that i manage to set the WDG_HALTin option byte 3.But the watchdog still resets the MCU after i enter halt. Please help me, cant i do it? If so then how do i read tha...

PRasm.3 by Associate II
  • 7164 Views
  • 15 replies
  • 0 kudos

Viper26LN 400V to 24V

Hello,I'am currently working on a implemented design out of the DesignStudio. The general purpose of the Viper26 in Buck Config is to supply another DCDC with 24V. Currently a load of 110 Ohm (Bleeder) Resistor is placed for testing purposes which re...

MNeun.1 by Associate II
  • 4361 Views
  • 7 replies
  • 0 kudos

Not able to debug - gdi-error [40412] Abort command is not possible in this CPU state (halt, wfi, protected code execution)

Hello Team I am using STVD IDE with cosmic compiler for development on STM8S207 series controller.I have two configurations in project called release and debug. whenever I try to debug code in debug configuration, following attached error appears whe...

SDalv.1 by Associate II
  • 2983 Views
  • 3 replies
  • 0 kudos