Spice Model for clt01_38q7
I want to simulate clt01_38q7 with LTSpice, but I couldn't find the spice mode in cad resources, so could you please provide it?
Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
I want to simulate clt01_38q7 with LTSpice, but I couldn't find the spice mode in cad resources, so could you please provide it?
I have been developing a project around the STM8S105 and I've been able to read and write the program and data memory fine several times (so I know that my STLink and dev board work well). Today I set the read-out protection to do some testing and af...
#include "stm8s.h" #include "stm8s_clk.h" #include "stm8s_adc1.h" #include "stm8s_gpio.h" #include "stm8s_tim2.h" #include "main.h" #include "flash.h" #include "stm8s_awu.h" volatile unsigned short _500ms_tick; volatile unsigned short idle_counte...
The Motor control firmware only generates header files. Please help me with the source code of the same, or any files if available. Thank you!
I have a common function that I use to set up Timer 5 (I'm using it for PWM output, if it matters):timerCounts = CLK_GetClockFreq() / pow(2, TIM5_PRESALER_xx) / pwmFrequency;TIM5_TimeBaseInit(TIM5_PRESCALER_xx, timerCounts);And that works really well...
Temperature range A = -40 °C to 85 °C and C = -40 °C to 125 °Cbut ST72F561J9TBXS Datasheet not mentioned suffix B temperature range, could you please share? thanks!
this eeprom i was wondering if there was an equivilant part and part number
Hello all,I have been checking this 30 kW Vienna PFC rectifier reference design and didn't understand why all of these filters are used for this kind of application, I mean half of the board is inductors and capacitors for the filters.Can someone exp...
Currently the project in which I am working requires a precision of milliohms and we would like to have this value to carry out calculations.