Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STEVAL-STRKT01 dimension

Hello everybody!Wish y´all a good day, i´m considering to use the STRKT01 for a project but before i buy it i need to know the physical dimensions of the module/development card, also the dimensions of the case that the kit includes. Thanks! 

stm8s003f

Can someone please help me to sort it out?Please I am stuck at a project.In the attached code I am unable to wake up the code  after sleep.Rest of the functions working once in sleep it shoild wakeup at if(MV>20)#include "stm8s.h" #include "stm8s_clk...

SRAM.11 by Associate III
  • 1765 Views
  • 2 replies
  • 0 kudos

sleep and wake up

for my code the sleep and wake up is happening simultaneously I need  the wake up  only on if(MV>20) and sleep if(MV<100) for a minute(low power mode)Please someone help to sort it out #include "stm8s.h" #include "stm8s_clk.h" #include "stm8s_adc1.h"...

SRAM.11 by Associate III
  • 1547 Views
  • 0 replies
  • 0 kudos

Resolved! "Error : Programming failed" while trying to program "STM8S103F3" microcontroller with "STVP"

I got a message "Error : Programming failed" while trying to program "STM8S103F3" microcontroller with "ST visual Programmer". Sometimes the microcontroller got programmed but several times it failed. I am using "ST-LINK V2" programmer (connections: ...

STM8programmingfail.png

S2-LP Hardware Control

We are using S2-LP Transceiver to wireless products of us. Our custom board has 2 layer and 1.6mm thickness and our operating frequency(OP) is 868 MHz. Also our output power is 14dBmUnfortunately we failed "Unwanted Emission in Spurious Domain" test....

wakeup function

Please some one help me to how to get controller from sleep the configuration I made is not working.The below given code working fine and putting the controller in sleep but controller not waking up.The condition depends on mains (ADC Input channel 5...

SRAM.11 by Associate III
  • 1299 Views
  • 0 replies
  • 0 kudos

Storing Data in EEPROM on the STM8S003k3

Hi Everyone,I am using stm8s003k3 in one of my projects. I want to store a variable containing a  number from 0 to 999 in EEPROM but the issue is FLASH_ProgramByte & FLASH_ReadByte can only store a number up to 256. I tried to use FLASH_ProgramWord b...

KRiaz.1 by Associate II
  • 1788 Views
  • 1 replies
  • 0 kudos