Resolved! Value of A8 bit in the EEPROM
Dear team, Please provide the A8 bit value of the following EEPROM M24C04-FMC6TG. Regards, Kaushal
Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
Dear team, Please provide the A8 bit value of the following EEPROM M24C04-FMC6TG. Regards, Kaushal
Hi, I am working to compile a pogam from the command line. The used compiler is the Cosmic compiler for the STM8 microcontrolerThe STVD Datasheet says that Export makefile ... | Generates a makefile script that can be launched with the gmake utility,...
Good morning,I write that post as remainder of a problem I encountered.In our embbeded software, the STM8 have to initialise EEprom with a bunch of default data on its first start.The process, that was working fine with previous ST7 now obsolete, fai...
Bonjour Tout le monde,J'ai une question a propos des interfaces disponibles avec lesquelles on peut tester une SPI, j'ai essaye PuTTY, termite avec un câble FTDI usb to mpsse (FT232H)(j'ai installé FT_Prog pour modifier la config de la chip du câble ...
Dear all,I need to the CMRT_Rev.6.31(Conflict Minerals Reporting Template) document.Best regard,Manamu Fukahori / SISTEC
Hello,i am currently testing the vl53l5cx lidar sensor without a coverglass, but i will need soon to use a coverglass(dusty environment). When using the coverglass, can the vl53l5cx (with Xtalk calibration) still detect object at close range(from 2cm...
Dear ST-Team, I am working on a STM8 MCU with the STVD. I want to compile my project in the Microsoft cmd line with a pipeline such as . cmd.exe /c "C:\Program Files (x86)\STMicroelectronics\st_toolset\stvd\stvdebug.exe" I haven't found any informati...
Hi,I'm evaluating ST8500 board, having purchased the complete kit Complete kit integrate an STM32G0 nucleo board that as my understanding is connected to ST8500 using UART (default baud 115200).I found out the G3 message format (header, checksum, pay...
Currently have the VL53V0X, Need a sensor that maintains high accuracy within the short distance as well as the long distance, speed is also a priority. I understand the Vl53L5CX has the multi zone distance sense, does it also work well as a single o...
Hi, I am having issue using a M24512RP in the exact same place as a M24512RT (I am talking of marking code on the chip). I2C EEPROM.From the datasheet it seems that 'T' suffixe is used to identify packing which would make sense for an ordering code, ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.