cancel
Showing results for 
Search instead for 
Did you mean: 

I have a Dell Optiplex 7020 which has an ST TPM version 1.2. In order to run Windows 11 I need to upgrade to a TPM version 2.0. Is it possible for the end-user to do the upgrade? If so, what part do I need for TPM version 2.0?

Paul.Sicard
Associate

The current specs are:

TPM Manufacturer version 13.12

PPI Specification Version 1.2

TPM specification sub-version 2,3

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome, @Paul.Sicard​, to the community!

Unfortunately, it is not possible to upgrade the TPM from 1.2 to 2.0 by simply exchanging the TPM chip, as it has to be supported by the BIOS/UEFI.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

Welcome, @Paul.Sicard​, to the community!

Unfortunately, it is not possible to upgrade the TPM from 1.2 to 2.0 by simply exchanging the TPM chip, as it has to be supported by the BIOS/UEFI.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.