cancel
Showing results for 
Search instead for 
Did you mean: 

About M95160

達井上.1
Associate

Does POR work even if the power is turned on slowly (even if the rise time is slow)?

No rise time is specified in the data sheet. 

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Mike_ST
ST Employee

Hello,

I don't see any restriction on that:

"5.1.2

At power-up, the device does not

respond to any instruction until VCC reaches the POR threshold voltage."

My interpretation is that there no time out for the POR feature.

The only constraint on VCC that I can see:

"5.1.3

The VCC voltage has to rise continuously from 0 V up to the minimum VCC operating voltage

defined under Operating conditions in Section 9."

達井上.1
Associate

Hello,​

Thank you for your reply.

Constraints pointed out 5.1.3

I think

"Continuous" = If the rising voltage does not increase or decrease temporarily due to noise etc.