User Activity

Hello, right now i am working with a STA8090 DevKit to test some things with the Teseo LIV3F. Unfortunatly, the software documentation is very inconsistent.For example in UM2399 Rev5 May 2020, there is the command$PSTMCFGCONST (page 151/376), which a...
Hello,i have a Nucleo-144 board, where i replaced the STM32F429ZI for a STM32F439ZI.I used CubeMX 5.2.0 to create a ethernet test project just to ping the board and go further from there, but i cant get it to work.Ethernet is enabledEthernet interrup...
Hello,i have a strange problem when i try to work with a FatFS on SD cards with SDIO.MCU is a STM32F439ZI, SDIO 4 wire for SD cards, FatFS for SD cards (used CubeMX 5.1.0 to create the base code, working with Atollic TrueSTUDIO 9.0.1)I have working c...
Kudos from