Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Accelerometer

Hello Team,We are using LSM6DSL in our device and want to increase the speed of reading data. We are not able to read accelerometer data more than 12.5 Hz with gyro initialization. Without the gyro initialization we are getting around 360 Hz data rea...

Afeefah by Associate II
  • 2007 Views
  • 1 replies
  • 0 kudos

ULN2804A SOC18

Hi, I can't find the ULN2804A with SMD SOC18 surface assembly, my question is,can I replace with the unl2803a SMD SOC18 ?n practice I have to repair an electronic card,I found all the components excluded the ULN2804A with surface assembly Soc18,which...

Franco1 by Associate
  • 2962 Views
  • 2 replies
  • 1 kudos

Resolved! Page write mode on M24C64-A125

Dear ST Community, Currently using the M24C64-A125 as EEPROM. We have a performance challenge in which we need to write a certain amount of data in less than 100ms. We checked the datasheet and we found out that The Page Write mode allows up to 32 by...

RachidBen_0-1697202747722.png
RachidBen by Associate II
  • 2949 Views
  • 4 replies
  • 0 kudos

SMPS Restart Problem

I have designed a 24v SMPS(switch mode power supply), but it is restarting what is the reason for that, I have used viper38hd IC.Here I attached my schematic, ic datasheet, and transformer datasheet.

Thivanka by Associate II
  • 8997 Views
  • 6 replies
  • 2 kudos

unintended internal discharge on STUSB4500?

Hi I have a design with the STUSB4500 per the attached schematic snippet and programmed per the attached memory map.  This circuit is on a tiny board inside the plug end of a captured USB cable. The PDO's are programmed to default to 20V @ 3A.The app...

Resolved! MTBF of ATECC608A-MAHDA-T

  Dear Technical Support, Could you provide me the MTBF of ATECC608A-MAHDA-T and the temperature which it was determined and the energy activation value? Thank you so much, María

Recommendation for STBC15LJ footprint

Hi,I'm planning to use STBC15LQ in a design, but I'm finding some contradictions between STM's AN4208 (an application note about flip chip bonding) and a very brief recommended footprint in the STBC15LQ datasheet.Can someone verify that the footprint...

ST10FLASHER translator to hex file

Posted on October 26, 2012 at 20:39As some of you may know, the ST10FLASHER provided by ST does not allow you to save target flash memory as an Intel hex file, but only as a formatted text file. For most, this may not be an issue, but I was in a sit...