Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM8S103F3 and OLED 128x32

Please I have mini board with processor STM8S103F3 and I need use I2C communication for OLED 128x32 panel SSD1306. Is there examples for ARDUINO IDE or STV Developer and Cosmic.Thank you very muchZdenek

Zdenek by Associate
  • 4762 Views
  • 2 replies
  • 0 kudos

two stm8s105c6t6 master and slave

Hi! i have two stm8105c6t6 , i want use one to master and other to slave, two pcb board are connect using 10k pull up resistor in the SDA/SCL line.  i am using the example AN3281 stm, but my microcontroller not have tim4, i change the tim4 to tim3 bu...

jdo by Associate II
  • 1505 Views
  • 1 replies
  • 0 kudos

M95020 not writing some bytes

I am trying to use the M95020 (M95020-WMN6TP to be exact) to replace older 2K SPI EEPROMs. Comparing everything in the data sheets seems to imply it should be a good replacement, with most tolerances higher than the old EEPROM.Yet for some reason, so...

tek00000.png tek00001.png tek00003.png