cancel
Showing results for 
Search instead for 
Did you mean: 

Teseo LIV3R connected to 3.3v but it does not send any commands, 1PPS always 0 and the module consumes 6 mA.

ABouk.1
Associate III
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
ABouk.1
Associate III

Vbatt and Vcc are both connected to a power supply that provides 3.3v.

Vcc_io is always connected to 3.3v (the same as the MCU) with a 22R resistor

RST, wakeup, 1PPS, TX and RX are connected to the MCU, however, the module does not send 11s pulses on 1PPS and it consumes 5.6 mA all the time.

RF_IN is connected to an active antenna and a LC circuit to provide the 3.3v.

I am really confused, No wrong connection have been made, is it possible that the module needs to be flashed ??