Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM8S103F3 programming error while using STVP

Hi All,This is my first post here and also my first interaction with ST micro devicesI'm truing to flash a .hex file into an STM8S103F3 using ST LINK V2 and STVP but I cannot connect to the device. I'm using a 5V external supply connected to the VDD ...

IMG_4109.JPG IMG_4110.JPG Capture.PNG

ST25R3920B-AQWT - reability details

Hello,Could you please send me all below details for ST25R3920B-AQWT ? Rev. of AEC-QHTOLTemp.-GradeHTOLTest-temperatureHTOLTest-durationSelf-heating Driving ChargingPrecondit-ioningOn-Grid ParkingOff-Grid Parking

HCori.1 by Associate
  • 1208 Views
  • 1 replies
  • 0 kudos

SPEAr1310

Good morning, I should reprogram a "SPEAr1310" do you have any device that does this?Thank you.

loris by Associate
  • 921 Views
  • 0 replies
  • 0 kudos

Resolved! STUSB4500 PDO SRC not read

Hi,I have a custom PCB with STUSB4500 as the UCPD controller and STM32H7 as my application processor. Without any I2C communication between stm32h7 and stusb4500 the stusb4500 is able to negotiate a higher voltage from a usbC PD source by matching it...

rd1987 by Associate II
  • 3532 Views
  • 4 replies
  • 0 kudos

Identify IC

Where can I buy this IC? I can't  find any information for it. If it is obsolete can you point me to the datasheet and alternatives?

image.png
bmateev by Associate
  • 984 Views
  • 0 replies
  • 0 kudos

STM8S103F3 and OLED 128x32

Please I have mini board with processor STM8S103F3 and I need use I2C communication for OLED 128x32 panel SSD1306. Is there examples for ARDUINO IDE or STV Developer and Cosmic.Thank you very muchZdenek

Zdenek by Associate
  • 4829 Views
  • 2 replies
  • 0 kudos

two stm8s105c6t6 master and slave

Hi! i have two stm8105c6t6 , i want use one to master and other to slave, two pcb board are connect using 10k pull up resistor in the SDA/SCL line.  i am using the example AN3281 stm, but my microcontroller not have tim4, i change the tim4 to tim3 bu...

jdo by Associate II
  • 1538 Views
  • 1 replies
  • 0 kudos