Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! IAR can not find STM8S103F2this chip

Hi teams,I want to use IAR(8.50)to develop STM8S103F2 series chip, but i can not find this chip at IAR setting, so how should I can do? download STM8S103 lib or others?thanks!

gavin3 by Associate II
  • 2668 Views
  • 2 replies
  • 0 kudos

Resolved! Trying to identify 14pin SOIC

Hello all, I am trying to debug a faulty board with two chips on it, which I am struggling to identify.Top row shows 324, bottom row does show the ST logo and "EZ7H713"Does someone have an idea where to look for a datasheet or even a pinout?

bombinho by Associate
  • 2108 Views
  • 2 replies
  • 1 kudos

Resolved! Unknow chip with ST logo (EZ945)

 Hi, Can anyone help please to identify what is this chip that hold the ST logo ? Here is the picture shows the chip.i searched a lot even on the digikey  but i couldn't find anything.thanks  

vrai_0-1700107121660.png
vrai by Associate II
  • 2157 Views
  • 1 replies
  • 1 kudos

Resolved! STD3PK50Z dc 2016

we just buy  STD3PK50Z  dc2016 but package look different is their any change ins pakage please share are this original please reply thanks  

peter_hk by Associate
  • 1933 Views
  • 2 replies
  • 0 kudos

Clarification on M99512 EEPROM

Hi,I hope to get clarification by the expert regarding the M99512 EEPROM - SPI connectivity. I recently had the chip together with Microchip AVR128DA64 mcu on a custom board. I found that at 500KHz communication with the eeprom, I can only store maxi...

STehA.1 by Associate II
  • 895 Views
  • 0 replies
  • 0 kudos

Resolved! Reverse engineering an membrane keypad

I have a machine which have 2 BLDC motors and I need to control it. I'm planning to control the motors by tapping the membrane keypad which already exists in the machine using microcontroller signal. I found the 2 pins that connected to certain butto...

jsw2000 by Associate II
  • 4518 Views
  • 7 replies
  • 0 kudos

MSL3 part not baked out prior to installation

I have a part LSM303DTR Accelerometer 3D Magnetometer that has an MSL rating of 3. This part was not baked out prior to installation on the PWA. What harm will this do to the component? If it passes testing, is it safe to use to go into space with (i...

MBuec.2 by Associate
  • 1168 Views
  • 1 replies
  • 0 kudos

Is it possible soft reset to 0x6000 bootloader?

Is it possible soft reset to 0x6000 bootloader?without control reset pin I try these codes doesn't work: FLASH_Unlock(FLASH_MemType_Data);FLASH_ProgramOptionByte(0x480B, 0x55);FLASH_ProgramOptionByte(0x480C, 0xaa);FLASH_Lock(FLASH_MemType_Data);#asmL...

chenxuuu by Associate
  • 1254 Views
  • 0 replies
  • 0 kudos

M27C64A-15F1

I have M27C64A-15F1 and M27C64A-15F1L, does anyone know what the difference is?The L suffix doesn't appear anywhere on the datasheet and I can't find any info on it ?

ASHLEA by Associate II
  • 2983 Views
  • 5 replies
  • 1 kudos