Can I know what is the max current rating per channel of the smart FET VNQ5050AK-E, it is quad channel IC and its total current is internally limited to 19A.
Hello Andrew,Thank you again for the quick support, its little confusing from the Graph(Figure 29) and then relating it too Table 6.Better is could you explain it with an example. I would be using this IC in 12V/24V system automotive environments.Tha...
Hello Andrew,Thank you for your reply, it helped me in understanding a little but the Tables you are referring in your explanation should I check it in Datasheet of IC, if yes than references you have made are not matching with that of datasheet.Than...