Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

PD55003L-E impedance related inquiries

Hello, my name is Choi Jae-yoon, and I am the Assistant manager of Sonartech in Korea.I have an inquiry regarding the impedance of the PD55003L-E product. 1. In the data sheet, impedance data is indicated only for the 480MHz to 520MHz frequency band....

Resolved! Finding a Mosfet suitable

I am building a high voltage fence controller, it requires a IRF820 Mosfet 500V 4A  N-channel. Apparently they are not manufactured anymore, and I can not find one anywhere, when trying to find out a replacement I am hitting brick walls with most peo...

5608920 by Associate II
  • 3036 Views
  • 4 replies
  • 0 kudos

ads1115 stm8 integration

hello,i am a beginner & i am trying integrate an external adc "ads1115" with stm8. the adc is an i2c device . i tried using peripheral library and also the register way. but its not working can anyone guide me the corect way to integrate this.this is...

niko27 by Associate II
  • 4610 Views
  • 7 replies
  • 0 kudos

Resolved! High frequency alternative to vn5e160str-e

I'm successfully using vn5e160str's to drive some high current outputs, but it would be useful if I could multi-purpose these outputs to support high frequency PWM. The vn5e160str seems to max out at about 50kHz, and I need a stable 800kHz.The PWMd l...

trullock by Associate
  • 1497 Views
  • 2 replies
  • 0 kudos

Resolved! Suggestion about (broken) F746ZG Nucelo Board

Good Morning,I am the proud possessor of a Nucelo 746ZG board that has served me well since it has been given to me.Unfortunately for ther last week the Nucleo has a text file with inside the string "The interface firmware FAILED to reset/halt the ta...

MMast.11 by Associate III
  • 2659 Views
  • 4 replies
  • 2 kudos

memory read failure

hi I am using M95512 512kb EEPROM connected to FPGA via SPI when Iam writing and reading the data (in single address(0000)) below sequence is followedstep 1: wren instruction is sending.(06)step 2: write data to memory array.(02)step 3: check WIP sta...

Renuka by Associate
  • 1184 Views
  • 1 replies
  • 0 kudos

Resolved! VIL Level of M74HC14YTTR IC

Hello, What is the VIL(Low Level Input) voltage of the IC M74HC14YTTR provided VCC voltage 3.3V?The datasheet specifies the VCC voltage levels of 2.0V, 4.5V, 6.0V. We have used the VCC as 3.3V.