I am importing a project that a colleague made. The project seems to be missing a lot of include files, I know I have the correct libraries in my repository but the project can't seem to find them. It seems like the filepath is pointing to C:/users/...
what's MSL OF STTH4R02S
The board appears in the list of devices as COM3 "STMicroelectronics Virtual COM Port". It is also present in the Configuration config of the UPWD application. What is the problem?
I am trying to generate high voltage pulses using STEVAL-IME013V1 but I could not manage so far. I applied;VDD=5V DCVSS=-5V DCHVP=HCP_CW= 20V DCHVM=HVM_CW= -20V DCWhen I use USB cable, the boards turns on, lights work fine, all buttons work. However...
I would like to know the location for download the latest firmware.When I put the phone, I have tried different brands smartphones it does not initiate to charge, it seams difficult to detect. The behaviour is erratic, sometime detect and start to c...
Hello, reading about the EMIF06-MSD02N16 datasheet it's quoting that it complies with IEC ESD 61000-4-2 Level 4 however the air discharge voltages quoted are 12kV. IEC 61000-4-2 specifies the air discharge Level 4 voltage as 15kV. Is this a typo, as ...
we are using STEVAL-IPFC01P1 load current is limited to 4A. If it is exceeded we Fault occurs and LED turns RED. Provide support in this regard