Others: hardware and software

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Error Amplifier Compensation Network Design

Hi, I'm using the converter Viper06 in my power supply board project. I'm having some difficulties to design the compensation network of the error amplifier. Could someone please tell me how to do this o share some documents that explains how t...

FLM.1 by Associate II
  • 953 Views
  • 2 replies
  • 0 kudos

Hi, Is it possible to have any mathematical dependencies, even approximate, between EEPROM FIT values and supply voltage? Thank you.

This might be a very basic question: EEPROM FIT values are based on standard single value of Ea = 0.7 eV. Is it irrelevant to supply voltage? I mean using lower supply for wide range device might reduce FIT values. Are any mathematical dependencies, ...

MLiou.1 by Associate II
  • 407 Views
  • 1 replies
  • 0 kudos

Hi, Does FIT of 2.4@90% 55°C/ ea=0.7 applies to higher reliability EEPROMs M24512-DRD3TP and M93C56-RDW3TP or they have has different FIT? Thank you!

Hi, I just got an answer for reliability of general parts EEPROMs M24512-DRD and M93C56-RDW. Thank you! Does 2.4@90% 55°C/ ea=0.7 applies to both _3TP and _6TP of M24512-DRD and M93C56-RDW, or M24512-DRD3TP and M93C56-RDW3TP has different FIT? 

MLiou.1 by Associate II
  • 432 Views
  • 1 replies
  • 0 kudos

STM704 battery switchover vs UL60950

Hello,We are using two components with unique coin cell backup. The first one is a RTC M41T93SMY6. For this one, I could find AN1011 that states that we don't need external diode and resistor to meet UL60950, it is built in the chip. The second one i...

HLepa.1 by Associate
  • 369 Views
  • 0 replies
  • 0 kudos

Dear, we have a problem whith some ST485BDR. When the 120 ohm load resistor is applied, the pin 1 goes to low state, lighting the green RX LED

This board perform 4 channels UART to RS485/422 conversion, using a FT4232 device and four ST485BDR devices. The issue is present in some channels in aleatory way. When I replace the failed ST485BDR device by the MAX485ESA the issued chanel start to ...

RMele.1 by Associate
  • 495 Views
  • 1 replies
  • 0 kudos