Automotive MCUs

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! SPC570S MCU running FreeRTOS freeze upon receiving CAN messages

Hi,I have a SPC570S MCU running FreeRTOS and is connected to a CAN bus. I came across an issue where the MCU freezes randomly, when there traffic in the CAN bus before is it switched on. Could someone help me in this matter. This happens randomly, an...

NBula.1 by Associate III
  • 978 Views
  • 3 replies
  • 0 kudos

Interrupt preemption - FreeRTOS

Dear all,I’m developing a system firmware for an engine ECU on SPC58EC microcontroller using FreeRTOS and SPC5Studio.During the tests I worked on interrupt priority and in particular I tested the correct servicing order of interrupt according to the ...

AParm.1 by Associate II
  • 873 Views
  • 2 replies
  • 0 kudos

Resolved! SPC5 compiling MCS code for SPC572L

We have a project running with TIM input signal and ATOM outputs and are now trying to use the MCS, we have looked at the GTM DPLL Test application and done some modification to the MCS program. Are there any tricks or options needed to compile the M...

Larsa by Associate II
  • 1232 Views
  • 4 replies
  • 0 kudos