Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

SPC560B ADC multiplexing

I want to use the PE7 pin of SPC560B to detect analog quantity​This requires reusing it as an ADC input pin​How should I configure him?

Jason Ren by Associate II
  • 1437 Views
  • 1 replies
  • 0 kudos

spc560 ADC can't read analog quantity

On spc560b MCU,I use PE [7] as ADC input,But why can't I read the analog quantityThere is no problem with the hardwareHow to configure the software part

Jason Ren by Associate II
  • 1786 Views
  • 2 replies
  • 0 kudos

[FCCU] use LONG_FUNC_RESET as a fault reaction. how to read fault information, such as which fault channel lead to this long functional reset, after reset?

we are trying to use LONG_FUNC_RESET as a fault reaction. However, I have a problem: how to read fault information, such as which fault channel lead to this long functional reset, after reset? From the FCCU RF_S/ N2FF_STATUS register?To analysis this...

0693W00000LviSvQAJ.png
bin zhuo by Associate II
  • 1140 Views
  • 1 replies
  • 0 kudos

Resolved! How to read the reset cause using MC_RGM register on SPC58NG84E7 controller?

Hello,I am currently working on SPC58NG84E7 controller with SPC5 studio.I want to read the cause of reset in main routine.In the reference manual, it is mentioned RGM register (RGM.FES & RGM.DES), which will help the controller to identify the type o...

AVM by Associate III
  • 2017 Views
  • 2 replies
  • 0 kudos

Resolved! Using a GTM / TOM as a source for eDMA

Hi all!!!I have a problem with GTM / TOM and eDMA.I am using a SPC58-BERNINA (STEVAL-TTM004V1) and SPC5Studio.My goal is to start a copy via eDMA channel when an interrupt of a TOM channel is triggered (suppose CN0 == CM0).In my example I am using GT...

_legacyfs_online_stmicro_images_0693W00000KdOPw.png _legacyfs_online_stmicro_images_0693W00000KdOSH.png
GFerr.5 by Associate
  • 1432 Views
  • 1 replies
  • 0 kudos

CAN channel initialization in SPC560B60

Hello,I am currently working on the SPC560b60 platform for my automotive application.I'm using a AUTOSAR CAN MCAL from ST. But i'm having trouble in initializing the CAN channels.The CAN channels seem to be always in a low power mode inspite of enabl...

SGori.1 by Associate
  • 2161 Views
  • 1 replies
  • 0 kudos

Resolved! Is it possible to not have a filter when receiving CAN messages?

Is it possible to not have a filter when receiving CAN messages? I want to create a gateway and transfer ALL messages from one CAN bus to another CAN bus. Do I just have to add 1000 messages to my list of allowed messages to ensure everything is acce...

PSing.5 by Associate II
  • 3020 Views
  • 2 replies
  • 0 kudos