Automotive MCUs

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

SPC582B60E1 CAN message filtering issue.

I am using dedicated Rx buffer and configured the filter to accept 3 CAN messages.For example,0x250 in Rx buffer 00x240 in Rx buffer 70x270 in Rx buffer 12Total number of Rx buffer used 32.Using MCAN Subsystem 0 MCAN 0. Shared RAM size is 3072. Stand...

DKuma.3 by Associate II
  • 525 Views
  • 1 replies
  • 0 kudos

Resolved! Incoherence in clock tree for SPC582 in SPC5Studio

Hello,I found unexpected behaviour in clock tree: when I change CGM_SC_DC2 divider - it affects another line in the diagram (the one with "FBRIDGE_CLK"). And when I change CMG_SC_DC3 divider - it affects the line above ("PBRIDGE_CLK").Best,Yannek

0693W000001qeTQQAY.png
Yannek by Associate III
  • 1670 Views
  • 7 replies
  • 1 kudos

SPC58XXADPT100S Hardware User Manual and Schematics

Hello,Could someone from ST side provide these two documents for the SPC58XXXADP100S minimodule? I have only the documents for 64 Pins and found there are some small hardware differences for the 100S. (Some Jumpers which are not mentioned in the doc...

bgong by Associate
  • 441 Views
  • 1 replies
  • 0 kudos

SPC572L complex ATOM output for direct injection

We have the basic structure up and running for our project with trigger signal input correct decoded and output timed correct throught MCS to the ATOM channels.ATOM outputs are now timed pulses of the right duration and position, but we would need to...

Larsa by Associate II
  • 504 Views
  • 1 replies
  • 0 kudos

Resolved! SIUL unit setting up

I want to implement the GPIO unit in the SPC560P50L5 microcontroller with the SPC5STUDIO IDE. Please advise me how to configure the SIUL unit and registers? Or give me an example of SIUL unit setting up in the SPC560P50L5 microcontroller.(I actually ...

Resolved! Hello, I'm trying to transmit and receive via DMA UART on SPC58EC-DISP. On the other side there is a STM32L432KC: the SPC transmit to STM32 which receives the message, but the message transmitted to SPC by the STM32 is not received. I post the code

#include "components.h"#include "serial_lld_cfg.h"void sddmatxcb(SerialDriver *sdp) { (void)sdp; pal_lld_togglepad(PORT_F, PF_LED2);}void sddmarxcb(SerialDriver *sdp) { (void)sdp; pal_lld_togglepad(PORT_F, PF_LED1);}/* * Application entry point. */in...

GGran.2 by Associate III
  • 577 Views
  • 1 replies
  • 0 kudos