Automotive MCUs

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! How to use eMIOS library for input capture

Hi,   I'm using SPC58EC Disp board. I want to use ultrasonic sensors with it. For that I have to config eMIOS as input capture mode. So, is there any example to config the libraries. If any kindly give it with some instructions. Thank You

Validation uC and quartz

For uC (SPC58EC74E1F0K0) we would like to verify its behaviour over time, via a simulation, with a new quartz circuit.Cand ST support?What is usually the lead time for such evaluation/simulation

VAlex.3 by Associate
  • 298 Views
  • 0 replies
  • 0 kudos

Resolved! Debug Options on spc5studio v6.0

Hello I installed spc5studio that downloaded from ST website and it works correctly. But in software, I can't debug MCU with spc5studio. I checked windows/preferences/Spc5studio ​ but there is not "Debug Options". How should I debug with spc5studio?

DNewm.1 by Associate III
  • 569 Views
  • 1 replies
  • 0 kudos

Resolved! SPC5-UDESTK not connect to SPC560B-DIS

Hi,I have SPC5-UDESTK plug in to SPC560B-DIS board and i have activated VCP but still not connect.If I use onBoard debbuger works, but i need to work with external SPT5-UDESTK to program my custom board, and indeed not work.Any idea?Thank you in adva...

Why there is no information on sta1295 (accordo5) ?

Hi Folks,I have been searching on the web or on the STM community for sta1295.I could not find any information apart from the data sheet.Don't even know where in the category to post this question? Can you folks please help understand this lack of in...

Configuration in spi slave mode

Hello.I'm working with spc560p and I want to enable it's spi slave mode​. All connections are OK but the slave is not working. My code is:​for(;;){spi_lld_start(...)​;spi_lld_receive(​...,Rxbuf);spi_lld_stop(...);​if(RXbuf == 0xAA){pal_togglepad;​}​}...

DNewm.1 by Associate III
  • 792 Views
  • 2 replies
  • 0 kudos

Resolved! SPC560P50L3 censorship issue

Hello,I purchased SPC560P50L3CEFAR from Mouser and I'm able to enable the censorship as the reference manual suggests.I'm modifying NVSCI0 and NVSCI1 registers with the value 0x55AABABA and the UDE cannot connect unless the correct password is provid...

NGuze.1 by Associate II
  • 855 Views
  • 1 replies
  • 0 kudos