Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Enable RTC driver on SPC560B discovery board (SPC5Studio)

I am using SPC5 Studio, version: 6.0 with an SPC560B discovery board. The onboard MCU is the SPC560B54L5. According to the datasheet this has an onboard RTC.I created a new project using the 'Create new SPC5 application' wizard. This works fine and I...

DColl.1 by Associate
  • 2090 Views
  • 1 replies
  • 0 kudos

SPC5 Studio osalThreadGetMicroseconds overflow

Hi,In the osal.c line 389 "osalThreadGetMicroseconds" function uses "osalSysTime_ST2US" macro to convert ticks to microseconds.The macro uses osalsystime_t variable type that is 32-bit length. return ((uint32_t)((((osalsystime_t)ticks) * 1000000UL) /...

sonerb by Associate II
  • 1395 Views
  • 1 replies
  • 1 kudos

UDE STK question.

I use a UDE STK .How do I check the value of a variable after creating a Braek Point ????​

hans536 by Associate III
  • 1084 Views
  • 1 replies
  • 0 kudos

SPC570S OTA update via CAN is not working

I'm working in a project, OTA update via CAN using esp32 and SPC570S. According to the application note the codes were made in the host side. The bootloader was modified to accept CAN frame and the addresses were set according to the application note...

kasun by Associate II
  • 1685 Views
  • 0 replies
  • 1 kudos

Need support for SPC58EG eMIOS as IPWM/ SAIC

Hello allcurrently we are trying to configure eMIOS channel for SAIC/ IPWM mode. all configuration for channels are correct.eMIOS 0 CH 19 , Mode = 2, BSL - D bus.Clock for eMIOS module up. Other channels which are configured for O/P functionalities ,...

VPhat.1 by Associate
  • 1516 Views
  • 1 replies
  • 0 kudos

Query regarding - SPC58EG DMA

We need your help regarding SPC58EG DMA configurations. We wanted configure DMA for DSPI communication.Below configurations are done in code , currently not working.eDMA_1 module , DMA channel – 12 (TX), 13 (RX), DMACHMUX_0 slot 6, 7 (as per below sn...

VPhat.1 by Associate
  • 1056 Views
  • 0 replies
  • 1 kudos

SPC58EN84C3 ADC test channel initialize error.

I tried to initialize test channels on SARADC_B (supervisor)./* Channels Configurations (DMA is not used)*/ static channelConfig _saradcconf_ch_configs[SPC5_SARADC_MAX_NUMOFCHANNELS] = { {SARADC_CHANNEL_TEST, 96U,SARADC_REFERENCE_DEFAULT, SARADC_PR...

0693W00000WKz9qQAD.png 0693W00000WKz4cQAD.png 0693W00000WKz9CQAT.png 0693W00000WKz92QAD.png
sonerb by Associate II
  • 1863 Views
  • 2 replies
  • 0 kudos