Automotive MCUs

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Port Pin Configuration Problem

Hi, on my SPC5 (SPHAERO) board, i set my pin configuration on port_I[1]But on "board.c" on board initialization component it state port_A. Anyone know why ? 

0693W00000QM2xwQAD.png 0693W00000QM2yuQAD.png
Angle by Associate II
  • 460 Views
  • 2 replies
  • 0 kudos

Hi ST Team, I want to load flash the SPC5 code via UART .So that I try to sue SPC5Flasher tool from following link https://www.st.com/en/embedded-software/spc5-flasher.html . I try to install it ask for serial number .

I requested serial number  but i am not able get serial no where can i get serial number.My requirement :- I want to flash bootloader and app code to SPC584B70E3CD00X MCU via UART.If any one have idea pls help me to solve.Thanks advanceRavi.S

Ravi S by Associate II
  • 653 Views
  • 1 replies
  • 0 kudos

HI ,, I AM USING SPC56EC64L8 FOR MY PROJECT. In Low Level Driver,only 0 to 7 and 24th emios channel is selsctable. we have written LLD for emios 10,11,13,14 which we are going to use. We found that there is no counter in these respective channels.

HI ,, I AM USING SPC56EC64L8 FOR MY PROJECT. In Low Level Driver,only 0 to 7 and 24th emios channel is selsctable. we have written LLD for emios 10,11,13,14 which we are going to use. We found that there is no counter in these respective channels. i ...

SPC5Studio-6.0.0-Clarke CDT

Hi,there is possibility that ST fix Build Output Parser (BOP) to have confortable IDE.Okay i can add :C:\SPC5Studio-6.0\eclipse\plugins\com.st.tools.spc5.tools.gnu.gcc.ppcvle.win32_4.9.4.20200908161514\toolchain\includeC:\SPC5Studio-6.0\eclipse\plugi...

Basic Context Switching problem

Hi There, i'm working on project to reduce blocking delay and i already use STM module for system time (system ticks) and preemtive of four thread using eTimer. But here i try to update a system where during delay it execute another thread immediatel...

MShaf.3 by Associate
  • 483 Views
  • 0 replies
  • 0 kudos

Resolved! DEBUG ERROR

Hi, anyone know how to fix this debug error ?

0693W00000QLD7BQAX.png
Angle by Associate II
  • 653 Views
  • 1 replies
  • 0 kudos

How do you set CAN Filter to allow only exact CAN IDs?

I am trying to set the CAN bus rx filter so that only the CAN message IDs that I specify in the can_lld_cfg.c file will be received. I tried to use the CAN classic filter setup for extended IDs. I set the mask to all ones (0x0fFFFFFFUL) so, it should...

SLam.1 by Associate
  • 600 Views
  • 0 replies
  • 0 kudos