Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

[solved]Pictus input pin selection

Posted on June 25, 2015 at 11:45Hello, Please see attached pictures cut from pictus RM0022 page 86. There are two input fucntion selectable of A[8] pin, SIN, and EIRQ[8]. I read and understand that to select input function , PCR.IBE = 1 must be set,...

270284440 by Associate III
  • 1427 Views
  • 2 replies
  • 0 kudos

Resolved! Flash memory write cycles

Posted on June 25, 2015 at 12:52Do ST have any data regarding Program/Data Flash write cycles and/or wear levelling for the SPC560B device(s)? I'd like to know if we have the option of using the Data Flash for built-in test logging on our SPC560B64.

How to change mcuconf.h values in the code generator?

Posted on June 26, 2015 at 15:34Hello, I always have to manually change some values in mcuconf.h when I generate the code out of the config because I can't find how to set them in the config or anywhere else. I'm using a 16MHz external xtal and I ha...

Probelm With License File in Spcstudio

Posted on June 02, 2015 at 07:59Hi one of my partners have problem with his windows when we re install a windows  and then install a spcstudio software when i run spc studio the error showed as in the picture. i have a license card and email what c...

SPC560D30L3 - Serial driver configuration

Posted on June 04, 2015 at 16:52I am using SPC560D30L3 with 8MHz crystal. The initialisation settings are as below,1. IDF = 12. NDIV = 483. ODF = ODF_DIV8I have configured the serial for 38400 baud with buffer for 16 bytes. I am trying to send a fra...

ssk by Associate II
  • 2816 Views
  • 11 replies
  • 0 kudos

SPC5Studio project settings

Posted on June 18, 2015 at 12:49Hello,I am using SPC5Stuido and the output file is generated as out.elf or out.hex etc. It is the default setting. I want to change it as per project need. From which project settings can I change the output file name...

ssk by Associate II
  • 1883 Views
  • 3 replies
  • 0 kudos

Resolved! SPC56EL54L3 not implemented in ''Platform Settings''

Posted on June 17, 2015 at 07:45Hello, For an upcoming project, I would like to use the SPC56EL54L3 controller. But when I was setting up a SPC5 Studio project, I can´t choose this controller in the platform settings because it is not listed. Is the...

Patriks by Senior
  • 2750 Views
  • 5 replies
  • 0 kudos

osal sleep

Posted on June 17, 2015 at 08:40Hello, I am a newer of SPC studio, while I am learning SPCstudio, I read help docs such as ''SPC560Pxx OS-less OSAL Component User Manual.chm'' I don't understand how this function ''osalThreadSleepMilliseconds(1000);...

Linker - incompatible section flags

Posted on June 10, 2015 at 10:52Hello,I am using SPC5Studio with SPC560D30L3 device. Till date I was able to build the project without any error/warnings. Recently I am getting a warning as below,4:10:08 **** Incremental Build of configuration Defau...

ssk by Associate II
  • 2176 Views
  • 3 replies
  • 0 kudos