I requested serial number but i am not able get serial no where can i get serial number.My requirement :- I want to flash bootloader and app code to SPC584B70E3CD00X MCU via UART.If any one have idea pls help me to solve.Thanks advanceRavi.S
In this I can able to download bin file from UART next step jump to app in this step not working if any one have idea please help .......Thanks advance ...
Hi sir,Sorry for the delay .Thanks for your replay.Now my code stat working .Logically how it work i don't know .may be some code generate issue.Just I done following think my code start working.1.Currently my code in Serial UART0 interface for code ...
Hi sir,I will check and update .But my doubt is LIN6 I configure can able to receive and send data with 115200bps .Only think code is not jump.any way i will change to LIN0 into my config then test and update the status .ThanksRavi.S
Hi sir,I attached the my bootloader code for your reference.Only difference from SPC5 example code I done following changes1.Defalt code CAN interface I changed to serial .2.I used LIN6 bard rate of 115200bps . Thanks Ravi.S
Hi sir,SPC584B LIN6 TXD D11 => RX on other MCU hostSPC584B LIN6 RXD D2 => TX on other MCU host Yes sir I connected this LIN6 only. big 4*37 connector X9 D1 and D11 pin connected to other MCU.Thanks Ravi.S