Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! SPC56EC64 MCU is resetting while using I2C moule.

We are using I2C of SPC56EC64 MCU to communicate with bq25798 battery charger IC.Communication is successfully done and we are also getting data from Charger.But whenever we do software reset of SPC56 MCU using below line of code mcu stuck in rese...

djtilava by Associate II
  • 4687 Views
  • 8 replies
  • 0 kudos

Resolved! spc56x series bootloader

Does the SPC560 can program in appilication (IAP) ?How CAN I do to implement the user bootloader? Is there any document about it? and the Chip has the BAM, is it means that ,I can user the factory bootloader to update the program via usart or FlexCan...

XDB.1 by Associate
  • 1920 Views
  • 1 replies
  • 0 kudos

Can I wake up spc58nh-disp by CAN module interrupt?

I use spc58nh-disp devel board.​I want to enter low power mode and wake up by CAN module interrupt.​How can i make "Wake UP" state through CAN module interrupt? How to setup??Are there any reference examples or resources??

hans536 by Associate III
  • 1318 Views
  • 2 replies
  • 0 kudos

SPC58EC-Disp standby mode entry and exit

Hello,I'm trying out standby mode application for spc58ec-disp board by using existing example code call WKUP. In that code stop mode is performed, but i tried with standby mode it fails.Is there any example code for standby mode?

Resolved! Wake up Example Question.

I am currently reviewing examples of the phrase 'WKPU'.Example is "SPC58xHxx_cut2_RLA WKPU Interrupt Test Application for Discovery".​If you press button sw0, LED3 turns on. If you press button sw1, LED1 turns on. And if you press button sw2, LED2 tu...

hans536 by Associate III
  • 4246 Views
  • 9 replies
  • 0 kudos

Resolved! Query on Stellar P or G series MCU

I am new to stellar MCUs. Please share information on how to get the SDK for stellar P series or G series MCU. Which IDE is used? Is there any RTOS support especially FreeRTOS support?

AVarg.8 by Associate
  • 2104 Views
  • 1 replies
  • 0 kudos

Resolved! Why RAM and System RAM shall be reset when system boot up?

Hi expert,I am using Stellar SR6 P7 line, e.g. SR6P7C8. According to the SDK there is RAM and System RAM reset operation when system boot,/* Initialize memories protected by ECC */ bl _raminit bl _sysraminitI want to get more information abou...

swu.1 by Associate II
  • 3280 Views
  • 4 replies
  • 0 kudos