Automotive MCUs

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! StellarStudio targetting SR6G7

Hello,I want to build a simple application (like a UART message, GPIO bit-bang etc.) targeting SR6G7 and running on a custom board. To support that I want to use the latest SDK 3.3.0 and flash the code via StellarLINK.Is there any guide how to add th...

savo by Associate
  • 885 Views
  • 1 replies
  • 0 kudos

Resolved! Set Life Cycle

I am using the SPC58 MCU product with the TRACE32 debugger. When changing the Life Cycle from "customer_delivery" to "in_field" with the trace32 script, debugging is only possible by entering the keycode. What should I do if I want to change the Life...

hgh by Associate
  • 752 Views
  • 1 replies
  • 0 kudos

Resolved! How to execute demo of sensorless Field oriented control in SPC560PL5 MCU and L9907 evaluation kit. There are three demos available 1 single shunt motor control 2 standard motor control 3 thee shunt motor control

How to execute demo of sensorless Field oriented control in SPC560PL5 MCU and L9907 evaluation kit. There are three demos available1 single shunt motor control2 standard motor control3 thee shunt motor control Which one should I select for sensorless...

PT.1 by Associate II
  • 729 Views
  • 1 replies
  • 0 kudos

Resolved! In SPC5 Studio, can we integrated imported example codes

I have tried to integrated imported examples in spc5 studio. I unbaled to done . Is there any setting you can help me..!!. I have used stm32cube IDE for stm32 series microcontrollers, it is very flexible and easy . Right now i am using spc570sxx se...

Rpasu.1 by Associate
  • 744 Views
  • 1 replies
  • 0 kudos

Maximum clock setting using Internal RC with SPC57

Hello, I would like to know how to configure Clock with SPC570S50E1, using internal RC oscillator.I would like to have maximum clock for each components. Currently, I succeed to set maximum system clock, but for ADC it is 1.6MHz while maximum is 12MH...

Noda_0-1703663112788.png Noda_1-1703663121113.png Noda_2-1703663132609.png
Noda by Associate
  • 657 Views
  • 2 replies
  • 1 kudos

SPC58N Memory Erase

Dear,I have SPC58N that writed wrong password on it, is it possible to blank memory and reprogram it with new software containing known password?Using PLS debug and JTAG Adaptor,regards,

Pilotdev by Associate
  • 356 Views
  • 0 replies
  • 0 kudos

Tools required for "AEK-AUD-C1D9031".

HiI came across  “AEK-AUD-C1D9031” which contain “SPC582B60E1”. For this I am looking for Flashing tool and Debugger with software.While searching for flashing tool and Debugger with software, I came across “SPC5-UDESTK USB/JTAG adapter” and  “SPC5-U...

Question about link script for SPC58EC80 with SPC5Studio.

Hello, I am currently using SPC58EC80 with SPC5Studio.I have some problem to load the data located in ROM area to RAM area when boot. I am using " > CAL_RAM AT > CAL_ROM" command for loading the data from 0x013A0000 to 0x400B0000.I check the RAM area...

otcagon by Associate II
  • 592 Views
  • 0 replies
  • 0 kudos

Resolved! difference between SPC5-UDEDEBG and SPC5-UDESTK-PLUS?

For starting with development on SPC56ELxx what I need is:the discovery board : https://www.st.com/content/st_com/en/products/evaluation-tools/product-evaluation-tools/mcu-mpu-eval-tools/spc5-automotive-mcu-eval-tools/spc56l-discovery.htmlSPC5 Studio...

gp73 by Associate III
  • 905 Views
  • 2 replies
  • 1 kudos