Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Wake-Up with CAN FIFO Rx in SPC5

Hi ST Team, MCU is SPC584B70E1. CAN0 is used as ISR-Rx normally. I want to choose "CAN FIFO 0 Rx New message Interrupt" as Wake-up Source. In SPC5 Studio, I configurated on WKPU Configuration setting , I selected INT 0 as WakeUp Source and in the CAN...

Gknr by Associate
  • 905 Views
  • 0 replies
  • 0 kudos

SPC564B74 input frequency measurements errors

Hi,I am using the SPC564B74 to measure the frequency of a square wave signal. The problem is that I have a some artifact measurements that cause problems on my application. A few times per minute, the measured frequency randomly drops to zero or an i...

SPC56 PMU not working

Hi!When I trigger the built-in LVD self-test for the Power Management Unit by writing PMUCTRL.CTRL.B.SILHT = 1, the PMUCTRL_FAULT register immediately indicates a low voltage detector fault and the MCU goes into SAFE mode. If I trigger the HVD test b...

DaveJ by Associate II
  • 925 Views
  • 0 replies
  • 0 kudos

Resolved! SPC560 Analog read of a pin

I'm searching for a simple API call such as found on Arduino :theValue = analogRead(port);does such a thing exist?  Hoping for pal_lld_analogReadpad( PORT_x, pinNumber );I find in adc_lld.h there is an array of functions which I am unsure why they ex...

Bucko_0-1726153376450.png
Bucko by Associate
  • 1644 Views
  • 1 replies
  • 1 kudos

SPC56 aborted FCCU operation

I want to clear the FCCU flags on my SPC56 chip. From the test application generated by SPC5Studio, I have the following code:static void spc_clear_fccu_rgm(void) {/* FCCU CF errors clearing.*//* Clear FCCU CF Status Register0 errors.*/FCCU.CFK.R = 0...

DaveJ by Associate II
  • 906 Views
  • 0 replies
  • 0 kudos

SPC56 Unclear instructions on using the STCU

I am developing a safety application on the SPC56EL60L3 platform. The reference manual RM0032 §43.1.3 outlines the steps for verifying the test results of the STCU (Self-test control unit). As I understand it, I first have to check the actual test st...

DaveJ by Associate II
  • 1333 Views
  • 1 replies
  • 0 kudos

Resolved! S19 Files in SPC5Studio

I believe the following question has been posted in the wrong label by @Nagendrapeddina , hence I am posting here as it has not been answered:How to generate .s19 file using SPC5 studio? Is it possible to generate .S19 files in SPC5 Studio ? 

asn by Associate III
  • 3501 Views
  • 6 replies
  • 6 kudos

How to generate .s19 file using SPC5 studio?

Hi All,I am using SPC50B60-L5 controller and spc5 studio (IDE) for building a project. And PEmicro multilink programmer for programming. I have built the project successfully. In build results I can see .hex, .elf, .bin out files but, I need .s19 fil...