Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! SPC5Studio Compatibility

I am currently using an SPC56P chip for my application. But I do not have an debugger probe for it which is compatible with SPC5Studio. So my question is: 1. Is SPC5-UDESTK-EVAL the only debugger probe that is compatible with SPC5Studio ? Or are ther...

asn by Associate III
  • 1986 Views
  • 3 replies
  • 1 kudos

Resolved! Can't update spc5studio - DNS problem

Some sites could not be found. See the error log for more detail.No repository found at http://hightec.spc5studio.com.No repository found at http://ai.spc5studio.com.No repository found at http://download.spc5studio.com/updates/.Error reading update ...

PWM Shutdown at Motor Terminals

I am usingSPC5 IDE with STEVAL-CTM009V1 (Eval Board) and STEVAL-TTM002V1 (Control Board), and want to implement braking; for that i want to know how can i shutdown PWM signals to motor? So that signals to my motor gets stop and it keeps running due t...

SPC58EC freeze after a while sending ethernet messages to linux

Hello to all, I'm working on a simple application for exchanging messages via ethernet with a SPC58EC. The application is a clean derivation of the gateway example without the remote which simply has to talk to another linux application.The applicati...

AMarc.9 by Associate
  • 2702 Views
  • 5 replies
  • 0 kudos

AEK-AUD-C1D9031 :I2S configuration

Hi, I'm using a FDA903D amplifier in my custom board . The I2S audio lines are giving proper output with  AEK-AUD-C1D9031 kit by passing the controller I2S lines to the FDA903D in my custom board (I have noted the CLK,WS, And SD lines as well). I'm t...

Resolved! Enabling the Multicore option in SPC574S64E3

I have been using the Eval L9963e board where i have SPC5764E3 ,Here in the below picture it is selected as Dual computing e200z4 core but i want to use one core the option is disabled can anyone give me the solution to this problem 

core.JPG