Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

SPC56 Unclear instructions on using the STCU

I am developing a safety application on the SPC56EL60L3 platform. The reference manual RM0032 §43.1.3 outlines the steps for verifying the test results of the STCU (Self-test control unit). As I understand it, I first have to check the actual test st...

DaveJ by Associate II
  • 817 Views
  • 1 replies
  • 0 kudos

Resolved! S19 Files in SPC5Studio

I believe the following question has been posted in the wrong label by @Nagendrapeddina , hence I am posting here as it has not been answered:How to generate .s19 file using SPC5 studio? Is it possible to generate .S19 files in SPC5 Studio ? 

asn by Associate III
  • 1898 Views
  • 6 replies
  • 6 kudos

How to generate .s19 file using SPC5 studio?

Hi All,I am using SPC50B60-L5 controller and spc5 studio (IDE) for building a project. And PEmicro multilink programmer for programming. I have built the project successfully. In build results I can see .hex, .elf, .bin out files but, I need .s19 fil...

Resolved! SPI Communication ( Single Master Multiple Slave)

Dear Community, I am working on an SPI-based setup where I have one SPI master and four SPI slaves, each connected to the master via their respective Slave Select (SS) lines. The configuration for the SPI master and the chip select lines is set up us...

Ali5_0-1726036518024.png
Ali5 by Associate III
  • 9436 Views
  • 4 replies
  • 3 kudos

SPC5 reset mode sets pin to high

I'm using the SPC5EC58 chip, and i want to switch some relays. This works so far. The problem is, during the reset mode even i'm setting it by Hardware like by a button or in the debugging mode, the pins which controlls the relays are set to high, ca...

PNeub.2 by Associate II
  • 609 Views
  • 0 replies
  • 0 kudos

How to disable censorship on a SPC572L

Hello,we have decided to protect our SPC572L based system via JTAG password protection, therefore we programmed the following data into flash:The 256 bit /8*32 bit JTAG password:00400120 11 12 13 14 21 22 23 24 31 32 33 34 41 42 43 44 00400130 51 52 ...

TomDoe by Associate
  • 879 Views
  • 1 replies
  • 0 kudos

interruptions and timer

good morning. i have a problem regarding button and time interrruptions. for the button, i linked it to the mcu but i do not know if i have to put the input as gpio or wake up, moreover, i do not know how to use the IRQ GUI, i do not know how it wor...

Jad_1-1725810905964.png Jad_2-1725810920505.png Jad_3-1725810940210.png Jad_0-1725812452419.png
Jad by Senior
  • 782 Views
  • 0 replies
  • 0 kudos

StellarStudio using Jlink Debug issue

Hi, I using the GDB SEGGER J-link with JTAG debug, and stuck in  "Setting breakpoint @ address 0x24001362, Kind = 2, Type = THUMB, BPHandle = 0x0001Starting target CPU..." Please help, thanks~      

BillyWu by Associate II
  • 1546 Views
  • 3 replies
  • 0 kudos

StellarStudio code optimization

Hello, Stellarstudio how to set the code optimization?  During the process of compiling a.C file into an.O file, the code is optimized. Commonly used optimizations include time optimization, which aims to make the code execution time shorter and more...

BillyWu by Associate II
  • 678 Views
  • 0 replies
  • 0 kudos