Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Help Needed: RTC Channel Configuration Issue on SPC58NN84

Hello team,I am currently working on configuring the GPT (General Purpose Timer) MCAL module for the SPC58NN84 microcontroller. While I have successfully configured PIT channels 0 and 1 for my project, I am encountering an error related to RTC (Real-...

Veer_1-1728382653353.png
Veer by Associate II
  • 1266 Views
  • 0 replies
  • 0 kudos

How to set the JTAG password lock for SPC584B?

I have successfully established a connection between SPC584B and UDE STK2 as shown below: Mo 07.10.2024 14:58:50.425, Success, Core2, UDEDebugServer, Connection to SPC584B70 target established: PowerPC Target, JTAG-ID: [32bit JTAG ID] In the UDE STK...

ishii by Associate
  • 1376 Views
  • 0 replies
  • 0 kudos

Unable to TX using CAN in SPC58NN84E4

Hi, I'm using the SPC58NN84E7 controller for CAN communication. I have referred the this application note that has a similar implementation for SPC58ECx controller. I have configured M_CAN_2_SUB_0 hardware channel for CAN communication with a baudrat...

vallabhd_0-1727956710102.png vallabhd_1-1727956887869.png vallabhd_2-1727957013400.png
vallabhd by Associate II
  • 1240 Views
  • 1 replies
  • 0 kudos

External flash interfacing with SPC582bxx MCU

Hello All, I am working on data storage on external flash memory, so for my application we are using SPC582Bxx MCU and W25QXX as external flash to store audio files into it. I have configured the below SPI pins to access the flash memory device, I ha...

RohitRajapure_0-1727951226150.png

Resolved! Can i run RTOS Task on Multi-core ??

I use spc58nh board.​I was using an RTOS Task On one core.​I want to use two core, and divide task into two cores.​​is this possible?for example : core2 - task 1, task 2 --> core 1 - task 1 , core 2 - task 2​

hans536 by Associate III
  • 2324 Views
  • 4 replies
  • 0 kudos

GTM DTM (Dead time Module) for SPC58NN84E7

Hello ST Community, I am currently working with the SPC58NN84E7 controller and using the AUTOSAR SPC58NN MCAL version 4.0.3.I am in the process of configuring the PWM module for our project, which requires both the GTM (for clocking the counter) and ...

Veer by Associate II
  • 1479 Views
  • 1 replies
  • 0 kudos

How to Enable Debugging for SPC584B70E1 in SPC5Studio?

Hello everyone,I’m currently working on a project using the SPC584B70E1 chip and SPC5Studio as my development environment. However, I’ve run into an issue where the “Execute” and “Debug” buttons are grayed out, and I’m not sure how to proceed. After ...

LEEDW by Associate
  • 963 Views
  • 0 replies
  • 0 kudos