Automotive MCUs

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

How to check stack and heap usage during run time.

Posted on February 16, 2018 at 06:03Hello Everyone,I am working on SPC560C50L3 MCU with SPC5 Studio. I am trying to add a library file which uses heavy stack and heap using dynamic allocations into my application. My code used to stuck in between du...

Resolved! How to disable Censorship on SPC560C50L3

Posted on February 08, 2018 at 11:55Hello Everyone,   I am working on SPC560C50L3 controller and using UDE STK 4.8 software for loading the firmware. I wanted to enable censorship. After going through the community I was able to get a code to erase ...

community.st.com

Posted on August 07, 2017 at 16:57SPC5Studio 5.5.0 is available Dear All ,SPC5Studio 5.5.0 is available*** Highlights ***Here are the changes coming with SPC5Studio v5.5.0For Mass Market: ===========-Sphaero (SPC574S) starter kit Platform component ...

Resolved! Shadow flash erase

Posted on October 05, 2017 at 16:00I need to programatically implement censorship on a SPC560B60x.  So this would involve unlocking and erasing the shadow sector and immediately writing new values for NVPWDx/NVSCCx.Unlocking involves LML[TSLK]/SLL[S...

SPC570S40 start in RUN0 mode with debugger

Posted on February 05, 2018 at 14:39Hi ,I'm new and I 'm developing on SPC570S40E1.I've a demo board and my final target board.When I try to debug my application I've 2 different behavior between  demo board and final target: on demo board during cl...

Safety SIL application and toolchain with SPC570S50E1

Posted on February 01, 2018 at 15:26Hello to everybody.I'm doing a research about different microcontrollers suitable for safety application, SPC570S50E1 is a very interesting candidate.The discussion is about what kind of support can I have for thi...

CFlash module example code for SPC560B60L7

Posted on January 31, 2018 at 01:17Hello!I'd like to use CFlash module without using C90LC Standard Software Driver(SSD).But I don't konw how to configure it.Could you provide me an example code?i.e) CFlash initialize, CFlash Erase, CFlash Write, et...

Hank Im by Associate II
  • 559 Views
  • 2 replies
  • 0 kudos

Resolved! Illegal instructions when using -fpic

Posted on December 22, 2017 at 09:55 Hello, I'm trying to make my application position independent so that I canplace the software anywhere in the flash of the SPC564B I'm using. Is this possible using the free FreeGCC v4.9.3 with VLE suppo...

Resolved! SPCSetRunMode not return ......

Posted on April 13, 2017 at 10:27 SPCSetRunMode not return ...... board: Discovery Plus Kit for SPC56 L line - with SPC56EL70L5 MCU my step: file->new sp5 studio Application wizard-> select Discovery Plus Kit for SPC56 L line - with SPC56E...

0690X00000606PiQAI.png 0690X00000606kdQAA.png 0690X00000606kxQAA.png 0690X00000606l2QAA.png

Resolved! Training/Tutorial about SPC5Studio

Posted on January 17, 2018 at 17:23Hi, I'm a new starter with ST MCU.Are there training/tutorial about SPC5Studio?Many thanks,Roberto#spc5studio #training #tutorial