Microcontrollers

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

The portMacro.h of FreeRTOS

Posted on August 28, 2017 at 06:15The MPC series is a 32-bit chip.Why is FreeRTOS portSTACK_TYPE defined as a long type? I think it should be uint32 type.Because STM32 is 32-bit chip, STM32 inside the portSTACK_TYPE defined as uint32 type

0690X000006081uQAA.png

[ATT]9313

Posted on August 24, 2017 at 14:46 Title Document: Tutorial : SPC5 FritzingHello SPC5 community ,we have created a new project SPC5Fritz available on githubhttps://github.com/microwan/spc5fritz this project is containing some parts for Fritzing tool...

0690X00000607klQAA.png 0690X000006080SQAQ.png

Resolved! Clocking SPC570

Posted on August 11, 2017 at 07:17Hi,i have a Problem with the Clock Configuration of the SPC570 �C (SPC570S-DISP). I just want to use the External Clock (crystal).my Configuration:CGM_SC_DC0/CGM_SC_DC1/CGM_SC_DC2 are set to 0x80000000AC0_SC/AC1_SC/...

Resolved! Can't activate FLASH/OTP Device !

Posted on August 16, 2017 at 11:06Hello community,I have 2 SPC56EL70L5-DISP boards and I am messing around with FlexRay.Today I was not able to program one of the boards anymore (with the same code as the other board).The UDE Memtool shows the error...

0690X00000607oDQAQ.png

FlexCAN Tx problem

Posted on July 17, 2017 at 08:50 Hello, I am working on a SPC560P Discovery Board. I have imported test application 'SPC560Pxx RLACAN Test Application for Discovery' for FlexCAN testing. In this FlexCAN0 is used in loop back mode and it is w...

Resolved! Low Level Interrupt Control Problem

Posted on November 04, 2014 at 12:58 Hello, I'm trying register base interrupt control. But not working.(problem *.s files) I do not want to use to OSAL library. Not starting interrupt. Example Code: //Orhan YILMAZ //Ti...

Resolved! SP5 Studio 5.5 Problem (CAN Issue)

Posted on August 10, 2017 at 04:321.The CANConfig structure adds a number of field information,it have a ''fifo_rx_callback'' function point.. Why is there a dialog box in SP5Studio that does not configure fifo_rx_callback?Causes the '' fifo_rx_call...

0690X00000607lhQAA.png 0690X00000607kVQAQ.png 0690X00000607n9QAA.png

Resolved! License check for trace stream failed for SPC560P50L5

Posted on June 16, 2017 at 08:05I am working on a CAN bus based project on the SPC560P50L5 platform. The project is based on the CAN RLA example included with the SPC5Studio.Details about my setup: SPC5Studio version 5.3UDE debug kit version 4.02.0...

Resolved! Unable to ''flash'' code to target

Posted on July 27, 2017 at 14:00Hi,I am using a SPC560C50L3 controller on a SPC560BADPT100S MINIMODULE board which sits on the XPC56XX EVB Motherboard. Power supply checked, jtag driver checked. The JTAG used is from PLS USB/JTAG Adapter for SPC5XXX...