Automotive MCUs

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

download.spc5studio.com

Dear All ,SPC5Studio updated components are available (56,57 on 58)more information on http://download.spc5studio.com/SPC58xHxx credentials should be requested on credentials@spc5studio.comNew or updated componentsCore 1.5.0   Pinmap wizard multiple ...

Resolved! How to handle interrupts in SPC5Studio generated application : boot.s in SPC56EL60L3 (HW/SW mode) ?

 * Unhandled exceptions handler for core 0.     */    .align   2    .weak    _IVOR0, _IVOR1, _IVOR2, _IVOR3    .weak    _IVOR4, _IVOR5, _IVOR6, _IVOR7    .weak    _IVOR8, _IVOR9, _IVOR10, _IVOR11    .weak    _IVOR12, _IVOR13, _IVOR14, _IVOR15    .wea...

Resolved! eclipse marktplace and check for updated Connection failed.

​After Installation of spc5 Studio, i want to download the toolchains. but there is always a Connection error. see below pls: org.eclipse.equinox.p2.transport.ecfWarningWed Mar 13 12:51:45 CET 2019Connection to http://vps182808.ovh.net:8080/marketpla...

bgong by Associate
  • 749 Views
  • 2 replies
  • 0 kudos

Resolved! Altium Designer libraries for SPC MCUs

Posted on February 12, 2016 at 09:33Hi everybody,does anybody know if SPC MCUs libraries are available for Altium Designer?Where could I find them?Thank you,Cel #spc #altium-designer #library

Resolved! Register Protection of SPC560Dxx

I do not quite understand paragraph 29.3 "Modes of operation" of RM0045 Reference Manual for SPC 56D Line MCUs. It says:Can my firmware change the protection dynamically, i.e. protect resp. unprotect registers?Is there any register that can get the s...

0690X0000087uE0QAI.png

Resolved! IBIS model - SPC584C

HiI would like to know if there is any IBIS models available for this devices?RegardsLin Biao

Resolved! Reset SPC56 without clearing RAM ?

Can I reset the device without losing memory contents at the same time? NOTE: This question and answer originated from a customer support case which was handled by us. We regularly review support cases and add any helpful ones here for all to benefit...

Resolved! Startup time of SPC560 B

We are using the SPC560B54L3 MCU in our project. After initial testing we found that the startup time is very high (about 235ms from powering the controller to the start of the application main function). From the documentation it is not clear how mu...

Resolved! How can i use the "stdio.h" at spc5 studio? ?

Hello. I use spc5studio and SPC582. i want use printf() using the UART for command line test. i alread tested serial. how can i setting  "stdio.h" header at spc5studio . ​please let me know code or seting.

BKIM.11 by Associate
  • 785 Views
  • 1 replies
  • 0 kudos