Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Element-to-element interference using 3-element VL53L0X array?

I'm using a linear array of 3ea VL53L0X sensors to orient a robot with respect to a nearby wall. The assumption is that when all three sensors return the same distance, then the robot is parallel to the wall. The sensors are mounted on a PCB with a ...

FPayn.1 by Associate III
  • 2293 Views
  • 2 replies
  • 0 kudos

Resolved! I'm getting faulty data from my vl53l5cx.

Most of the target status seem to return 5 but some do return 255.The data is correct on all 64pixels when I have a near object (200mm) but it cannot detect further objects like the ceiling and instead it will return a seemingly random small distance...

LCord.1 by Associate III
  • 3105 Views
  • 5 replies
  • 0 kudos

Interfacing two VL53L0x ToF sensors with an ATmega328p in AVR C

Hello,I've got a question.I'm trying to interface two VL53L0x ToF sensors with an ATmega328p board. This worked fine in the arduino IDE with the beautiful Adafruit library. Unfortunately this library does not work in AVR C so I'm trying to create the...

ev.1 by Associate
  • 2942 Views
  • 2 replies
  • 0 kudos

Using the VL53L1x API with the controller that I use

I am using a TI simplelink controller. How do I go about using the VL53L1 APIs with my controller code. I am guessing I need to use STSW-IMG007 software. I can't use this software directly. How should I go ahead with interfacing it? Any guidance will...

VBhag by Associate II
  • 1587 Views
  • 2 replies
  • 0 kudos