Skip to main content
dlux
Associate II
May 6, 2022 8:39 PM UTC
Question

Upload VL53L5CX firmware to multiple targets on the same bus at the same time?

Hi,

i have multiple VL53L5CX sensors on the same bus. Right now i am initializing the firmware (vl53l5cx_init) them after setting the individual I2C addresses. I wonder if it is possible to initialize them all at once.

To my understanding the vl53l5cx_init transfers the code that runs on the internal microcontroller to it via the I2C bus. That should in theory work as kind of a broadcast transfer.

Thank you in advance.

This topic has been closed for replies.

1 reply

Anne BIGOT
ST Technical Moderator
May 10, 2022 9:50 AM UTC

Hello

In the current case (setting the individual I2C addresses first), to load the firmware you will need to give the individual I2C address of the sensor. Only one sensor at a time can be addressed. You can not initialize all the sensors at once.

If you try to load the firmware first, inside the initialization function there is a polling to know when the firmware is ready. If you have multiple sensors sharing the same bus with the same address, you cannot know which sensor is ready. This is important to respect the timescale and instruction sequence of the driver initialization which is not possible to meet with several sensors sharing the same I2C address.

So in this case, you can not initialize them all at once.

Anne

Our community relies on fruitful exchanges and good quality content. You can thank and reward helpful and positive contributions by marking them as 'Accept as Solution'. When marking a solution, make sure it answers your original question or issue that you raised. ST Employees that act as moderators have the right to accept the solution, judging by their expertise. This helps other community members identify useful discussions and refrain from raising the same question. If you notice any false behavior or abuse of the action, do not hesitate to 'Report Inappropriate Content'