Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X,Y and Z coordinates for X-NUCELO-53L1A1 TOF sensor.

Hello everyone,so I am using the X-NUCLEO-53L1A1 TOF sensor and I want to detect the height ( Z) of objects that it detects but in the examples I found it only shows information about the objects' range ( distance Y) so my question is : Is there a w...

WYous.1 by Associate III
  • 6199 Views
  • 7 replies
  • 0 kudos

Why I can't get vl53l0x to work with RAK3172?

Hello guys, I am trying to use VL53L0X with old version of VL53L0X API (There is an issue with new version aapi with windows.h). Status always returns -20. Why is that? My Code;/* USER CODE BEGIN Header */ /** **************************************...

I wanted to insert a ToF sensor (VL53L4CD) in an anesthetic container, I wanted to know which types of glass are suitable with the sensor.

I wanted to insert a ToF sensor (VL53L4CD) in an anesthetic container, because of the influence of the anesthetic on the sensor I need to protect my sensor with a protective glass, I wanted to know which types of glass are suitable with the sensor (c...

kdass.1 by Associate
  • 1528 Views
  • 2 replies
  • 1 kudos

Do all VL53L* sensors use the same VCSEL with the same power?

I was wondering if all the VL53L* sensors use the same VCSEL illumination source with the same average and peak power. I would think the the long-range sensors (VL53L1CB) and the sensors with wide FoVs of 63 degrees, would need a more powerful VCSEL.

FGuti.2 by Associate II
  • 1201 Views
  • 1 replies
  • 0 kudos

Sensor init failed on using VL53L1X ultra low power driver

We have been using the full driver for VL53L1X and would like to try out the new ultra low power driver on our board. Everything works fine with the full driver. However, we are facing a problem on VL53L1X_ULP_SensorInit() when using the ultra low po...

ALai.1 by Associate II
  • 2333 Views
  • 2 replies
  • 0 kudos

VL53L1X orientation and ROI

Dear,I want to implement a people counting algoritme using the VL53L1X ToF sensor. I want to build my own PCB for it. I found out that when the sensor is rotated by 90 degrees (gold filters in a row), the edges of a door are measured better then when...

SBann.1 by Associate II
  • 1292 Views
  • 1 replies
  • 0 kudos

Resolved! PerformRefSpadManagement doesn't work

This is the detailed log of the I2C communication between an ESP32 and a VL53L4CX[I][logger:242]: Log initialized [VV][esp32.preferences:070]: nvs_get_blob: key: 233825507, len: 4 [C][ota:469]: There have been 0 suspected unsuccessful boot attempts. ...

IHern.2 by Associate III
  • 4104 Views
  • 8 replies
  • 0 kudos