Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Finding the VL53L1X XTALK calibration distance

I am trying to perform the XTALK calibration for my system that includes a coverglass on top of the sensor. I am not exactly sure what the point of calibration should be. I've read in the forum: "When doing crosstalk calibration you need to find a ta...

0693W00000Y8QTuQAN.png 0693W00000Y8QUEQA3.png 0693W00000Y8QysQAF.png
MRoso.1 by Associate II
  • 3828 Views
  • 6 replies
  • 0 kudos

Timing budget not kept in VL53L1X

I am trying to get consecutive measurements from the VL53L1X sensor but the timing budget is only kept on the first measurement with the below codeVL53L1X_BootState(dev, &sensorState); VL53L1X_SensorInit(dev); VL53L1X_SetDistanceMode(dev, 2); VL53L1X...

0693W00000Y8L5PQAV.png
MRoso.1 by Associate II
  • 4388 Views
  • 8 replies
  • 0 kudos

VL53L1X range status 4 on long range

I'm trying to measure distance in a very dark environment. I'm using long-range distance mode. Suddenly, the sensor started sending error 4. What can cause this and how to fix it?Fixed, caused by an issue in the code.

SBann.1 by Associate II
  • 2698 Views
  • 4 replies
  • 0 kudos

Signal threshold not working as expected?

I'm using a VL53L1X ToF sensor to measure distance with the Ultra Lite driver. I've lowered the signal threshold to 400 because that value seems to cover most valid measurements. When I read the current signal value using GetSignalRate(). When my sig...

SBann.1 by Associate II
  • 2955 Views
  • 6 replies
  • 0 kudos

Resolved! vl53l5cx_set_ranging_frequency_hz and TOF sensors

The datasheet says the maximum ranging frequency's for VL53L5CXV0GC/1 are 60Hz at 4x4 15Hz at 8x8But the firmware allows for example perfectly 100Hz at 4x4 by setting this value with vl53l5cx_set_ranging_frequency_hz().I also can see the sensor is re...

sde c.1 by Senior II
  • 1362 Views
  • 1 replies
  • 0 kudos

Generate interrupt with VL6180 while MCU is sleeping

EDIT: Figured it out, I had to run the VL6180 in continuous mode.I'm using a VL6180 for hand detection. I've successfully set up the interrupt at a certain range and it works nicely when the MCU is running. When the MCU is not running (aka not pollin...

CRett.1 by Associate
  • 1156 Views
  • 1 replies
  • 1 kudos

Resolved! VL53L3 and Sunlight

Hello,I have a problem with VL53L3 sensor measurements. When sunlight hits the sensor, the measurement is distorted, and the measured distance becomes small. Are there any settings for the sensor to remove this glitch when the sun's rays hit?

Vandr.1 by Associate II
  • 1364 Views
  • 1 replies
  • 0 kudos