Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! VL53L5CX Target Order Values

When I use vl53l5cx_get_target_order, it returns 2.I assume there are only two values (1 & 2). Does 2 = CLOSEST or Strongest?Thanks.Giri

GRama.2 by Associate III
  • 1520 Views
  • 1 replies
  • 0 kudos

Resolved! Vl53L5CX - cause of stop_ranging() to fail

I am encountering a strange problem on the VL53L5CX sensor. Here is the rundown of my setup:3 sensorseach gets initialised and new i2c address is set so they can run simultaneouslyturn all sensors on and wait for external inputThe external input is s...

ALohr.1 by Associate II
  • 2990 Views
  • 4 replies
  • 0 kudos

Resolved! VL53L0X food oil measurement in metal can

hello.I am trying to measure the level of cooking oil in a metal container using the VL53L0X chip.The length and width of the metal container are 25 cm and the height is 35 cm.Please refer to the picture for detailed measurement environment. However,...

DES.png

Question regarding enabling/disabling Crosstalk Compensation

Hello. I am seeking to perform a series of tests to demonstrate the effect of enabling/disabling the cross-talk compensation on the VL6180x ToF sensor. For some context, I'll be setting targets of different reflectance across different distances and ...

AGome.7 by Associate II
  • 1609 Views
  • 1 replies
  • 0 kudos

Using DMA for communication with ToF sensor VL53L7CX

Hello,Standard library for ToF sensors, as far as i know, works in blocking mode and it needs few seconds to initialize sensor and later on to gather all of 64 results. In my project I need to handle other process during this time and using DMA seams...

MŻbik.1 by Associate II
  • 2014 Views
  • 2 replies
  • 0 kudos

VL6180 proximity detection logic output mode

Hi, I would like to know if we can configure GPIO0 or GPIO1 as a logic output mode. In datasheet, we can configure in INT mode. But we need to clear the flag each time we have a value. So we have a wrong value during the clearing. I would like to con...

ELECL.2 by Associate II
  • 1508 Views
  • 1 replies
  • 0 kudos