cancel
Showing results for 
Search instead for 
Did you mean: 

Would a 'time of flight' sensor such as the VL53L4CD detect snowflakes or rain?

GPres.1
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
John E KVAM
ST Employee

No - I don't think so.

While visiting Calgary Canada on a really cold day, I spent a lot of time ranging on snow.

The VL53L1X that I was using at the time, simply did not see the snow.

940nm light is absorbed by water vapor - it's why there is less 940nm light than other frequencies at the surface of the earth. It's also one of the reasons we chose that frequency.

The sensor can see a pool of water because the surface acts a bit like a mirror. But rain drops and snowflakes don't reflect the photons the way the water surface does.

  • john

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.