cancel
Showing results for 
Search instead for 
Did you mean: 

VL53L5CX: minimum size of an empty zone between 2 objects

EPARM.1
Associate

Hi, I'd like to know what is the minimum size or gap between 2 objects the sensor is able to detect ? My first test shows a surface of 600 cm² seems to be the minimum, i.e a "hole" square of 25 cm x 25 cm or a rectangle of 20 x 30 cm.

When I do the math for the size of the 8x8 zone the result is a resolution of 15x15 cm. Why is there this important diffference ? Any parameter to setup ?

Thanks

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
John E KVAM
ST Employee

Lots of stuff going on here.

The FoV is a bit short of 45x45. So an 8x8 would assume about a 5 degree by 5 degree FoV for each zone. And that's about as accurate as we get.

Now a really bright object will 'splash' onto it's neighbors. It's why we have a sharpener.

The best thing to do is experiment with the Evaluaiton kit, and try different sharpener settings.

Turning it down guarentees you don't miss small targets. Turning it up tightens the edges.

Find a setting that makes you happy. Not everyone will agree on the best depending on what one is looking for.

  • john

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.