Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! More questions about Size of Zones and FoV

I have a very simple question concerning the size of the zones and the field of view for (for example) the VL53L8CX sensor. which has a diagonal FoV of 65 degrees. Can anyone provide a simple answer to this question:If the sensor is 1 meter from the ...

Guy1 by Associate II
  • 1401 Views
  • 1 replies
  • 0 kudos

Resolved! Which API should vl6180 use?

HI, i am studying how to controll vl6180 with a custom board which MCU is STM32L452CCU6. At the beginning , i tried to avoid implementing the api by changing register directly using i2c, however,0x018 is set to 0x2 or 0x0 both did not generate the ra...

LCHAN.41 by Associate II
  • 1805 Views
  • 1 replies
  • 1 kudos

Resolved! About overcome indirect sunlight problem with vl6180X/V1?

Hey, I am using a customize board (MCU:STM32L452CCU6) to develop a gate checker with vl6180/V1 and cover glass with IR filter. Implemented a default value and setting ,the sensor and code works fine indoor. But in the outdoor condition under the sunl...

LCHAN.41 by Associate II
  • 1751 Views
  • 1 replies
  • 0 kudos

Resolved! VL53L5CX gesture library older versions

Hi, I would like to download older versions of the VL53L5CX gesture library (to be exact the 1.7 and 1.8 versions for cortex M4), but I'm only allowed to download the latest one (1.9). Is there any possibility to download these two versions?Regards.S...

SOsle.1 by Associate
  • 1839 Views
  • 1 replies
  • 0 kudos

Resolved! VL53L1X Recommended conditions for offset calibration About 140mm

Hello,I am developing a system using VL53L1X.I have read UM2356 (VL53L1X API user manual).I would like to know the background of the recommended conditions for the offset calibration procedure Chart distance: 140mm.Is it a peculiar point that Chart d...

KArai.2 by Associate II
  • 2304 Views
  • 2 replies
  • 1 kudos

Resolved! Problem with the new VL53L1X

In my product I use the VL53L1X sensor for more than 2 years. But the last 50 sensors I bought had a problem. The measurement is too incorrect and the peak_signal_count_rate_MCPS and ambient_count_rate_MCPS parameters are too low. I purchased sensors...

test.jpg

Resolved! VL53L5CX out of range values not returning to 0 for zones that are looking into open space areas, has anyone else seen this issue?

I’ve used the VL53L1X and found it to be very reliable, I obtained a few VL53L5CX the (Sparkfun Breakout version) for assessment to a particular project.A similar issue has been logged on the Spark fun forum a couple of years ago without any resoluti...

_legacyfs_online_stmicro_images_0693W00000dK2LRQA0.png _legacyfs_online_stmicro_images_0693W00000dK2LbQAK.png _legacyfs_online_stmicro_images_0693W00000dK2EgQAK.png
SMcAn.1 by Associate
  • 4062 Views
  • 4 replies
  • 1 kudos

Resolved! Limiting data sent from the VL53L5CX I am trying to upgrade the ultrasonic distance sensors on a Heathkit 2000 robot. Its baud rate is 9600, so it could be overwhelmed by an 8x8 data array sent at 60 Hz.

Is it possible to have a computer ask the sensor for only certain pixels when it is needed?From what is posted by your vendor Sparkfun, the data array can be 4x4 or 8x8, and repetition rate can be 1, 15, or 60Hz. Are these options set by the approxim...

MBres.1 by Associate
  • 3688 Views
  • 4 replies
  • 0 kudos