Skip to main content
Simon86
Associate
April 25, 2019
Question

Does X-CUBE-AI supports the ARM Compiler 6.12?

  • April 25, 2019
  • 0 replies
  • 1139 views

Hello,

I am using CubeMX 5.1.0 with the X-CUBE-AI 3.4 package. It works really fine with Atollic TrueStudio and the GCC. However, the perfomance / runtime of our algorithm is not satisfactory, so that we would like to use the ARM Compiler 6.12 to look if the duration of the algorithm would be faster. Unfortunately, I got some Linker-Errors when I try to use the Keil MDK with ARM Compiler 6.12 and I saw that the Lib-File "network_runtime.lib" is pre-compiled with ARM Compiler 5.06.

Is there another file "network_runtime.lib" for ARM Compiler 6.12?

If no, when will CubeMX and X-CUBE-AI support the ARM Compiler 6.12?

Thanks.

Best Regards,

Simon

This topic has been closed for replies.