Edge AI

Ask questions and find answers on how to deploy, debug, and optimize AI models on ST microcontrollers, microprocessors, and smart sensors.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

[Short Survey] Please give us your feedbacks on ST model Zoo Services

Hi everyone,   In order to help our developers understand how their work is used and what to do in order to improve model zoo, we kindly ask you to look at this survey about ST Model Zoo Services.   Link of the survey: https://docs.google.com/forms/d...

MLC Output Delay

Hello,I have recently conducted a test on the activity recognition task using the ST library with ESP32 MCU. Although it functions correctly, there are noticeable delays before action recognition occurs. I am seeking advice on how to address this iss...

FKara.3 by Senior
  • 1343 Views
  • 1 replies
  • 0 kudos

error when analyzing the .onnx model in stm32cubeMX by stm32cube.AI

Hi, Thanks for your attention. I am analyzing the .onnx format model but an error occurs. I try to reinstall the stm32cubeMX but it doesn't help. The part of architecture is: Here is the log information. Can you help me with this problem? @Romain LE ...

0693W00000QKl99QAD.png 0693W00000QKlBZQA1.png
BHuan.3 by Associate III
  • 8436 Views
  • 9 replies
  • 1 kudos

X-CUBE-AI: what is the input buffer format?

Hi,I'm trying to test X-CUBE-AI on my Stm32F429ZI nucleo board. I'm using Stm32CubeMX, Stm32CubeIDE.Setup: stmnist_v1.h5, I've PNG files for this dataset.At first I'd like to test the AI routines with in-memory buffer so I'd like to know what is the ...

Test User by Associate III
  • 3484 Views
  • 0 replies
  • 0 kudos

Artificial intelligence on raspberry pi

Hi team. May you kindly assist how to eliminate false positive for a face recognition project  is it my code which is the problem or something else. For white people I am getting true positives but for blacks, only false positives.

Inaccurate step count vales while using LSM6DSOX built in pedometer

Hi,I am currently using LSM6DSOX and its features like MLC and built in pedometer in a project, MLC works just fine but when I am walking whilts LSM6DSOX is in a 40 to 50 degrees tilted position on my wrist, pedometer misses around half of the steps ...

enis_isik by Associate II
  • 1191 Views
  • 0 replies
  • 0 kudos

Resolved! Updated CubeAI can't find Runtime

I've updated my code to CubeAI 8.1. The middleware is still deleted... but I can add it manually. However when I build the code I gett the error:Description Resource Path Location Typecannot find -l:NetworkRuntime730_CM7_GCC.a AI_FILES_GENERATOR C/C+...

KSOdin2_0-1689857782573.png KSOdin2_1-1689857823405.png KSOdin2_2-1689857862226.png
KSOdin2 by Associate III
  • 5101 Views
  • 1 replies
  • 0 kudos

Resolved! Analog output from MLC in lsm6dsv16x

Hello,Can we generate analog output from MLC instead of a statement? If we can, could you explain how to do it? I plan to use MLC output as a part of my control algorithm. What is the most efficient way to achieve this?

FKara.3 by Senior
  • 1494 Views
  • 1 replies
  • 0 kudos

I am starting an APP with AI

Hello good afternoon, I am starting to make an application with the sensortile.box very similar to "baby crying". I would like to ask if you have any information that can support me in this process, for example to activate the use of the AI folders i...

SAbba.1 by Associate III
  • 1636 Views
  • 1 replies
  • 0 kudos

About Yolov5 being unable to be deployed on CubeAI when transitioning to Onnx

我真的不知道为什么..将出现此问题。将 YOLOv5 转换为 ONNX 后,我无法在其上部署它,因为我的显卡是 1660ti 并将半精度转换为单精度。如果我使用半精度,它可能不支持 16 位半精度(所以要减小我的权重文件的大小并不容易),但如果我切换到单精度,则意味着列表溢出,并且没有指示溢出发生的位置。我真的很相信,事实上,我还没有看到一些 Yolov5 部署在 cubeAI 上......一些大人物知道为什么在这里

微信图片_20230714085808.png 微信图片_20230714085752.png